:MEASure:EYE:RN:LEVel
Flex Apps:
FlexDCA
Meas. mode:
Eye
Package License:
L-RND
Licensed Feature:
F-AEYE
Waveform type:
NRZ
PAM4/6/8
Command Syntax
:MEASure:EYE:RN:LEVel {LEVel0 | LEVel1 | LEVel2 | LEVel3}
Query Syntax
:MEASure:EYE:RN:LEVel?
Description
Selects the eye diagram's level on which to perform the RN measurement. The LEVel2 and LEVel3 arguments apply only to PAM4 signals. If you experience difficulties measuring a PAM4 signal, confirm that the signal-type setting is set to PAM4 with the :CHANnel:SIGNal:TYPE command.
Requires Option 401, Advanced Eye Analysis Software license.
Requires FlexDCA revision A.05.30 and above.