:MEASure:EYE:RN:RNSTabilize

Flex Apps:
FlexDCA
Meas. mode:
Eye
Waveform type:
NRZ
PAM4/6/8

Command Syntax

:MEASure:EYE:RN:RNSTabilize {ON | OFF}

Query Syntax

:MEASure:EYE:RN:RNSTabilize?

Description

Turns on or off RN stabilization for the RN measurement. When RN stabilization is on, use the :MEASure:EYE:RN:RNSValue command to enter the RN value. To measure the RN, switch the N1000A to Jitter Mode and measure the RN while using a signal that has a short pattern. Or, measure the RN using a separate instrument. The following list shows that the eye mode DI, Jn, RN, and TI measurements each have RNSTabilize and RNSValue child commands. Because the RNSTabilize commands control the same setting, you can use any of the four commands to turn RN stabilization on or off. Also, because the RNSValue commands enter or query the same variable, you can use any of the four commands to change or query the RN value.

Linked RN Stabilization (On / Off) Commands

The following list shows that linked RNSTabilize commands the DI, RN, and TI measurements. The RNSTabilize command for any of these three measurements turns RN stabilization on or off for all three measurements (DI, RN, and TI).

Requires Option 401, Advanced Eye Analysis Software license.

Requires FlexDCA revision A.05.30 and above.