:MEASure:EYE:TDEC:OMA:VALue

Flex Apps:
FlexDCA
FlexRT
Meas. mode:
Eye
Waveform type:
NRZ

Command Syntax

:MEASure:EYE:TDEC:OMA:VALue <amplitude>

<amplitude> is a double.

Query Syntax

:MEASure:EYE:TDEC:OMA:VALue?

Description

Enters the result of Oscilloscope mode's OMA measurement (:MEASure:OSCilloscope:OMAmplitude command. This OMA value is used when measuring TDEC with the :MEAS:EYE:TDEC command. In order for this value to be used in the TDEC calculation, you must select a user-defined definition as set by the :MEAS:EYE:TDEC:METHod sibling command. The query form of the command returns the user-defined OMA value.

Requires FlexDCA revision A.05.00 and above.