:MEASure:EYE:VECP:OMA:VALue
Meas. mode:
Eye
Waveform type:
NRZ
Flex Apps:
FlexDCA
FlexRT
Command Syntax
:MEASure:EYE:VECP:OMA:VALue
Query Syntax
:MEASure:EYE:VECP:OMA:VALue?
Description
Enters the result of Oscilloscope mode's OMA measurement (:MEASure:OSCilloscope:OMAmplitude command. This OMA value is used when measuring VECP with the :MEAS:EYE:VECP command. In order for this value to be used in the VECP calculation, you must select a user-defined definition as set by the :MEAS:EYE:VECP:METHod sibling command.
The query form of the command returns the user-defined OMA value.
Requires FlexDCA revision A.05.50 and above.