:MEASure:JITTer:OJITter:JRMS:DISPlay
Flex Apps:
FlexDCA
Meas. mode:
Jitter
Waveform type:
PAM4
Meas. panel:
Output Jitter
Command Syntax
:MEASure:JITTer:OJITter:JRMS:DISPlay {ON | OFF | 1 | 0}
Query Syntax
:MEASure:JITTer:OJITter:JRMS:DISPlay?
Query Response
{ON | OFF | 1 | 0}
Description
Controls the display of the IEEE JRMS measurement results in the displayed Output Jitter panel. Select ON, the default value, to expand the panel to show EOJ measurement results for all edges. Select OFF to contract the panel so that only the EOJ measurement result made for all edges is visible. When OFF is selected, only the JRMS result for all edges can be queried using the :MEASure:JITTer:OJITter:JRMS? query. To move the results to the top of the panel, use the :MEASure:JITTer:OJITter:JRMS command.
Requires FlexDCA revision A.05.70 and above.