:MEASure:JITTer:POJitter:LIST:SELect

Flex Apps:
FlexDCA
Meas. mode:
Jitter
Waveform type:
NRZ
PAM4
Meas. panel:
Timing Jitter
Timing Jitter

Command Syntax

:MEASure:JITTer:POJitter:LIST:SELect <integer>

Where <integer> is identifies a measurement row. For example, 2.

Query Syntax

:MEASure:JITTer:POJitter:LIST:SELect?

Query Response

<integer>

Description

In Jitter Mode's Timing Jitter panel for Phase-Only Jitter, selects a measurement in the panel's table.

Requires FlexDCA revision A.08.30 and above.

Example Command

:MEASure:JITTer:POJitter:LIST:SELect 1