:MEASure:JITTer:POJitter:STATe
Command Syntax
:MEASure:JITTer:POJitter:STATe {ON | OFF | 1 | 0}
Query Syntax
:MEASure:JITTer:POJitter:STATe?
Query Response
{ON | OFF | 1 | 0}
Description
Sending ON activates the following Phase-Only Jitter measurements for PAM4 signals. You can use these commands to query the measurement results based on all edges or specific edges.
- JH4u (
:MEASure:JITTer:POJitter:JH4u) - JHrms (
:MEASure:JITTer:POJitter:JHrms)
Activating these commands displays the measurement results in the Timing Jitter panel and displays the Raw RJ/PJ Histogram. Selecting the histogram to be displayed does not affect the measurement results shown in the panel or returned by the commands. Sending OFF turns off all Phase-Only Jitter measurements. To include the Timing Jitter panel results in the documentation wizard, use the :DISK:DWIZard:POJitter:SDATa command.
Always follow this command with the :SYSTem:AUToscale and *OPC? command to start the measurements.
:MEASure:JITTer:POJitter:STATe ON :SYSTem:AUToscale *OPC?
Requires FlexDCA revision A.08.30 and above.