:MEASure:MARKer:DY?
Meas. mode:
Scope
Eye
TDR
Flex Apps:
FlexDCA
FlexRT
Query Syntax
:MEASure:MARKer:DY{1:4}{A:C}?
This command supports the STATus? and STATus:REASon? common child commands.
Description
Queries the difference in time between any two Y-axis markers, whether they are tracking marker pair or manual line markers. The two markers can have different source waveforms. Use the :MARKer subsystem to turn on markers. To display or hide the Δ Position and Δ Magnitude listings in the displayed Markers table, use the :DISPlay:MARKER:DELTas command.
Requires FlexDCA revision A.03.00 and above.
Example Command Sequence
:MARKer:Y1A:SOURce CHAN2A :MARKer:Y2A:SOURce CHAN2B :MARKer:Y1A:STATe MANual// Marker 1 turned on as a manual line marker :MARKer:Y2A:STATe TRAC// Marker 2 turned on as a tracking marker pair … :MEASure:MARKer:DY2A?