:DISPlay:MARKer:DELTas
Instrument:
N1000A
DCA-M
Meas. mode:
Scope
Eye
Jitter
TDR
Flex Apps:
FlexDCA
FlexRT
Command Syntax
:DISPlay:MARKer:DELTas {ON | OFF | 1 | 0}
Query Syntax
:DISPlay:MARKer:DELTas?
Query Response
{1 | 0}
Description
Shows or hides the Δ Pos (delta position) and Δ Mag (delta magnitude) listings in the displayed Markers table. This is equivalent to clicking Show Δ Values in the table. To return the Δ Pos measurement, use the :MEASure:MARKer:DX? query. To return the Δ Mag measurement, use the :MEASure:MARKer:DY? query.
Requires FlexDCA revision A.03.00 and above.