:MEASure:MARKer:IDX?
Query Syntax
:MEASure:MARKer:IDX{1:4}?
This command supports the STATus? and STATus:REASon? common child commands.
Description
Queries the reciprocal of the DX? marker measurement. The two markers can have different source waveforms. Use the :MARKer subsystem to turn on markers.
Requires FlexDCA revision A.03.00 and above.
Example Command Sequence
:MARKer:X1:SOURce CHAN2A :MARKer:X2:SOURce CHAN2B :MARKer:Y1A:STATe TRAC// Marker 1 turned on as a manual marker :MARKer:Y2A:STATe TRAC// Marker 2 turned on as a waveform tracking marker … :MEASure:MARKer:IDX2?
Measurement Ready?
To confirm that the measurement is ready to read, you can query the measurement's status:
if ('CORR' in Flex.query(':STATus?')):
measurement = Flex.query('?')
If averaging is turned on (:ACQuire:AVERaging), you can also confirm if the measurement result is ready by comparing the number of specified averages (:ACQuire:ECOunt?) versus the number of measurement sweeps that have occurred (:COUNt?). The technique uses the :COUNt? common measurement query. For example,
if (Flex.query(':COUNt?') >= Flex.query(':ACQuire:ECOUNt?')):
measurement = Flex.query('?')
You can also use an acquisition limit lest to test that a number of waveform samples, or pattern acquisitions have completed before returning a measurement. Refer to the :LTESt:ACQuire:CTYPe command.
Common Measurement Child Queries
This command supports the use of the following common measurement queries: :LOCation?, :COUNt?, :MAXimum?, :MINimum?, :MEAN?, and :SDEViation?.