:MEASure:MARKer:Y:STATus?
Meas. mode:
Scope
Eye
TDR
Flex Apps:
FlexDCA
FlexRT
Query Syntax
:MEASure:MARKer:Y{1:4}{A:C}:STATus?
Query Response
{CORR | INV | QUES}
- CORR
- The measurement result is correct.
- INV
- The measurement result is invalid. A question mark (?) is shown in the displayed results table instead of a measurement result.
- QUES
- The measurement result is questionable. A question mark (?) is shown in the displayed results table next to the measurement result.
Description
Queries the status of the Y measurement. Use the STATus:REASon? child query to determine the reason for a invalid or questionable measurement.