:MEASure:MARKer:Y?
Query Syntax
:MEASure:MARKer:Y{1:4}{A:C}?
This command supports the STATus? and STATus:REASon? common child commands.
Description
This command queries the amplitude of a Y-axis manual-line marker or tracking marker pair. In TDR/TDT mode, with S-parameter magnitude, phase, and group delay waveforms displayed, you can create one tracking marker at an X value that has three different Y values, one from each waveform at the same X value. In other words, this single tracking marker has three Y values at the same X position. All three Y values are shown in additional Magnitude columns in the marker results table. The following table shows how to identify the Y values in the query. Each waveform is identified using a letter from A to C.
| Y Value | Example Marker 2 Query |
|---|---|
| Magnitude Y Value | :MEASure:MARKer:Y2A? |
| Phase Y Value | :MEASure:MARKer:Y2B? |
| Group Delay Y Value | :MEASure:MARKer:Y2C? |
To turn on a marker, use the commands in the :MARKer subsystem.
Example Command Sequence
:MARKer:Y1A:SOURce CHAN2A :MARKer:Y1A:STATe TRACking … :MEASure:MARKer:Y1A?
Measurement Ready?
To confirm that the measurement is ready to read, you can query the measurement's status:
if ('CORR' in Flex.query(':STATus?')):
measurement = Flex.query('?')
If averaging is turned on (:ACQuire:AVERaging), you can also confirm if the measurement result is ready by comparing the number of specified averages (:ACQuire:ECOunt?) versus the number of measurement sweeps that have occurred (:COUNt?). The technique uses the :COUNt? common measurement query. For example,
if (Flex.query(':COUNt?') >= Flex.query(':ACQuire:ECOUNt?')):
measurement = Flex.query('?')
You can also use an acquisition limit lest to test that a number of waveform samples, or pattern acquisitions have completed before returning a measurement. Refer to the :LTESt:ACQuire:CTYPe command.
Common Measurement Child Queries
This command supports the use of the following common measurement queries: :LOCation?, :COUNt?, :MAXimum?, :MINimum?, :MEAN?, and :SDEViation?.