:MEASure:OSCilloscope:DELTatime:REGion

Flex Apps:
FlexDCA
Meas. mode:
Scope
Waveform type:
NRZ
PAM4/6/8

Command Syntax

:MEASure:OSCilloscope:DELTatime:REGion {DISPlay | REGion{1:8}}

Query Syntax

:MEASure:OSCilloscope:DELTatime:REGion?

Description

Select a time span over which the :DELTatime measurement is made.

DISPlay
The measurement is performed on the displayed portion of the waveform. This is the default selection.
REGion{1:8}
The measurement is performed across one of eight regions. Regions are defined using the :MEASure:REGions:STATe command.

Example Command Sequence

:SYSTem:MODE OSCilloscope
:MEASure:OSCilloscope:DELTatime:SOURce1 CHAN1A
  //  Defines first measurement edge
:MEASure:OSCilloscope:DELTatime:ENUMber1 2
:MEASure:OSCilloscope:DELTatime:EDIRection1 RISing
:MEASure:OSCilloscope:DELTatime:ETHReshold1 MIDDle
  //  Defines second measurement edge
:MEASure:OSCilloscope:DELTatime:SOURce2 WMEMory1
:MEASure:OSCilloscope:DELTatime:ENUMber2 3
:MEASure:OSCilloscope:DELTatime:EDIRection2 FALLing
:MEASure:OSCilloscope:DELTatime:ETHReshold2 MIDDle
  //  Select measurement region
:MEASure:OSCilloscope:DELTatime:REGion DISPlay
  //  Perform measurement
:MEASure:OSCilloscope:DELTatime
:MEASure:OSCilloscope:DELTatime?