:MEASure:REGions:STATe
Command Syntax
:MEASure:REGions:STATe {ON | OFF | 1 | 0}
Query Syntax
:MEASure:REGions:STATe?
Query Response
{1 | 0}
Description
Enables and displays all defined measurement regions in Oscilloscope Mode. Measurement regions allow you to restrict the data used for a measurement to a specific area of the source waveform as defined by left and right X-axis limits. Up to eight measurement regions can be specified. Use the :MEASure:REGions:COUNt command to specify the number of regions. Use the :MEASure:REGions:REGion:X{1:2} command to set the x-axis boundaries for each region.
After defining one or more regions, use the :REGion child command of a specific measurement to apply a region to the measurement. For example, limit a rise-time measurement to the data within region 3, use the following command:
:MEASure:OSCilloscope:RISetime:REGion REGion3
Requires FlexDCA revision A.01.70 and above.
Measurement regions are only available in Oscilloscope and TDR modes.
The Jitterp-p and Jitterrms measurements can not be made on a measurement region.
Example Command Sequence
:SYSTem:MODE OSCilloscope :MEASure:REGions:COUNt 1 :MEASure:REGions:REGion1:X1 40E-12 :MEASure:REGions:REGion1:X2 100E-12 :MEASure:REGions:STATe ON :MEASure:OSCilloscope:RISetime:SOURce CHAN1A :MEASure:OSCilloscope:RISetime:REGion REGion1 :MEASure:OSCilloscope:RISetime :MEASure:OSCilloscope:RISetime?