:MEASure:OSCilloscope:DUTYcycle:REGion

Flex Apps:
FlexDCA
Meas. mode:
Scope
Waveform type:
NRZ
PAM4/6/8

Command Syntax

:MEASure:OSCilloscope:DUTYcycle:REGion {DISPlay | REGion{1:8}}

Query Syntax

:MEASure:OSCilloscope:DUTYcycle:REGion?

Description

Select a time span over which the :DUTYcycle measurement is made.

DISPlay
The measurement is performed on the displayed portion of the waveform. This is the default selection.
REGion{1:8}
The measurement is performed across one of eight regions. Regions are defined using the :MEASure:REGions:STATe command.

Example Command Sequence

:SYSTem:MODE OSCilloscope
:MEASure:OSCilloscope:DUTYcycle:SOURce CHAN2A
:MEASure:OSCilloscope:DUTYcycle:REGion REGion3
:MEASure:OSCilloscope:DUTYcycle
:MEASure:OSCilloscope:DUTYcycle?