:MEASure:OSCilloscope:PAM:LEVel:LEVel

Flex Apps:
FlexDCA
Meas. mode:
Scope
Waveform type:
NRZ
PAM4

Command Syntax

:MEASure:OSCilloscope:PAM:LEVel:LEVel {LEVel0 | LEVel1 | LEVel2 | LEVel3}

Query Syntax

:MEASure:OSCilloscope:PAM:LEVel:LEVel?

Description

Selects the level of a PAM4 or NRZ signal that will be measured when the :LEVel parent command is sent. PAM4 signals have four possible levels: 0, 1, 2, and 4. NRZ signals has two possible levels: 0 and 1.

Arguments Description
LEVel3 Selects level 3.
LEVel2 Selects level 2.
LEVel1 Selects level 1.
LEVel0 Selects level 0.

Example Command Sequence

:MEASure:OSCilloscope:PAM:LEVel:LEVel LEVel2

Requires FlexDCA revision A.04.50 and above.