:MEASure:PAM:AMPLitude:UNITs
Meas. mode:
Eye
Scope
Package License:
L-RND
L-MFG
Waveform type:
PAM4
Flex Apps:
FlexDCA
FlexRT
Command Syntax
:MEASure:PAM:AMPLitude:UNITs {AMPLitude | PERCent}
Description
Sets the amplitude units for PAM4 level and level RMS (thickness) measurements. The selections are amplitude (volts or Watts) or percent. The following measurements are affected by this setting:
- Eye/Mask Mode
- PAM Levels (
:EYE:PAM:LEVel) - PAM Levels RMS (
:EYE:PAM:RMS) - PAM Eye Levels (
:EYE:PAM:ELEVel) - PAM Eye Heights (
:EYE:PAM:EHeight) - Oscilloscope Mode
- PAM Levels (
:OSCilloscope:PAM:LEVel) - PAM Levels RMS (
:OSCilloscope:PAM:RMS)
To select the units for Jitter measurements (seconds or unit interval), use the :MEASure:JITTer:DEFine:UNITs command.
Requires FlexDCA revision A.04.50 and above.