:MEASure:OSCilloscope:TVOLt:EDIRection
Flex Apps:
FlexDCA
Meas. mode:
Scope
Waveform type:
NRZ
PAM4/6/8
Command Syntax
:MEASure:OSCilloscope:TVOLt:EDIRection {RISing | FALLing}
Query Syntax
:MEASure:OSCilloscope:TVOLt:EDIRection?
Description
For the Time-at-Amplitude measurement, specifies the edge direction used to identify the waveform location at which to perform the measurement. The edge can be identified as rising or falling. To specify the edge number, use the :OSCilloscope:TVOLt:ENUMber command. To specify the amplitude value, use the :OSCilloscope:TVOLt:YVALue command.
Example Command Sequence
:SYSTem:MODE OSCilloscope :MEASure:OSCilloscope:TVOLt:SOURce CHAN1A :MEASure:OSCilloscope:TVOLt:EDIRection RISing :MEASure:OSCilloscope:TVOLt:ENUMber 1 :MEASure:OSCilloscope:TVOLt:YVALue 100E-03 :MEASure:OSCilloscope:TVOLt :MEASure:OSCilloscope:TVOLt?