:MEASure:OSCilloscope:TVOLt:YVALue

Flex Apps:
FlexDCA
Meas. mode:
Scope
Waveform type:
NRZ
PAM4/6/8

Command Syntax

:MEASure:OSCilloscope:TVOLt:YVALue  <amplitude>

<amplitude> is a double.

Query Syntax

:MEASure:OSCilloscope:TVOLt:YVALue?

Description

For the Time-at-Amplitude measurement, specifies the amplitude value at which to perform the measurement. To specify the edge direction, use the :OSCilloscope:TVOLt:EDIRection command. To specify the edge number, use the :OSCilloscope:TVOLt:ENUMber command.

Example Command Sequence

:SYSTem:MODE OSCilloscope
:MEASure:OSCilloscope:TVOLt:SOURce CHAN1A
:MEASure:OSCilloscope:TVOLt:EDIRection RISing
:MEASure:OSCilloscope:TVOLt:ENUMber 1
:MEASure:OSCilloscope:TVOLt:YVALue 100E-03
:MEASure:OSCilloscope:TVOLt
:MEASure:OSCilloscope:TVOLt?