:MEASure:PEYE:ESKew:EYE
Flex Apps:
FlexDCA
Meas. mode:
Jitter
Waveform type:
PAM4
Meas. panel:
Eye
Command Syntax
:MEASure:PEYE:ESKew:EYE {EYE0 | EYE1 | EYE2}
Query Syntax
:MEASure:PEYE:ESKew:EYE?
Description
This command allows you to select an eye on PAM4 signals. For NRZ signals, the 0 eye is automatically selected and cannot be changed. The command selects the PAM4 eye on which to perform the :MEASure:PEYE:ESKew. The query form of the command returns the currently selected eye.
Requires FlexDCA revision A.06.00 and above.