:MEASure:PEYE:ESKew:SOURce

Flex Apps:
FlexDCA
Meas. mode:
Jitter
Waveform type:
PAM4
Meas. panel:
Eye

Command Syntax

:MEASure:PEYE:ESKew:SOURce <source_waveform>

Where <source_waveform> can be one of the following:

  • CHANnel{1:8}{A|B|C|D}
  • DIFF{1:4}
  • CGMemory{1:8}
  • FUNCtion{1:16}

Query Syntax

:MEASure:PEYE:ESKew:SOURce?

Description

Selects the source waveform on which to perform the :MEASure:PEYE:ESKew measurement.

Requires FlexDCA revision A.06.00 and above.