:MEASure:PEYE:EWIDth:EYE

Flex Apps:
FlexDCA
Meas. mode:
Jitter
Waveform type:
PAM4
Meas. panel:
Eye

Command Syntax

:MEASure:PEYE:EWIDth:EYE {EYE0 | EYE1 | EYE2}

Query Syntax

:MEASure:PEYE:EWIDth:EYE?

Description

This command selects the eye on which to perform the :EWIDth measurement. The query form of the command returns the currently selected eye. The results are placed in the following results table:

  • Jitter table for NRZ signals.
  • Eye table for PAM4 signals.
PAM4 Waveform

This is a command for PAM4 signals only. For NRZ signals, this command results in an "−221, Settings conflict " error.

Requires FlexDCA revision A.06.00 and above.