:MEASure:PLEVel:LINearity:SOURce
Flex Apps:
FlexDCA
Meas. mode:
Jitter
Waveform type:
PAM4
Meas. panel:
Level
Command Syntax
:MEASure:PLEVel:LINearity:SOURce <source_waveform>
Where <source_waveform> can be one of the following:
CHANnel{1:8}{A|B|C|D}DIFF{1:4}CGMemory{1:8}FUNCtion{1:16}
Query Syntax
:MEASure:PLEVel:LINearity:SOURce?
Query Response
<source_waveform>
Description
Selects the source waveform on which to perform the measurement.:MEASure:PLEVel:LINearity
Requires FlexDCA revision A.06.40 and above.