:MEASure:PLEVel:SNDRatio:LOCation?
Flex Apps:
FlexDCA
Meas. mode:
Jitter
Waveform type:
PAM4
Meas. panel:
Level
Query Syntax
:MEASure:PLEVel:SNDRatio:LOCation?
Description
Returns an index for the location of the SNDR measurement results in the active measurement list. Using this information, you can select, clear, or remove measurement results from the displayed results table. If the measurement is not listed in the table, a "−1" is returned.
Requires FlexDCA revision A.07.90 and above.
Example Command
:MEASure:PLEVel:SNDRatio:LOCation?