:MEASure:TDR:RISetime:REGion
Instrument:
N1000A
Flex Apps:
FlexDCA
Meas. mode:
TDR
Waveform type:
T-Parameter
S-Parameter
Command Syntax
:MEASure:TDR:RISetime:REGion {DISPlay | REGion{1:8} }
Query Syntax
:MEASure:TDR:RISetime:REGion?
Description
Select a time span over which the :RISetime measurement is made.
- DISPlay
- The measurement is performed on the displayed portion of the waveform. This is the default selection.
- REGion{1:8}
- The measurement is performed across one of eight regions. Regions are defined using the
:MEASure:REGions:STATecommand.
Requires FlexDCA revision A.04.00 and above.
Example Command Sequence
:SYSTem:MODE TDR :MEASure:TDR:RISetime:SOURce TRACe4 :MEASure:TDR:RISetime:REGion REGion1 :MEASure:TDR:RISetime :MEASure:TDR:RISetime?