:MEASure:TDR:VAVerage:LOCation
Instrument:
N1000A
Flex Apps:
FlexDCA
Meas. mode:
TDR
Waveform type:
T-Parameter
S-Parameter
Query Syntax
:MEASure:TDR:VAVerage:LOCation?
Description
Returns an index for the location of the VAVerage measurement results in the active measurement list. Using this information, you can select, clear, or remove measurement results from the displayed results table. If the measurement is not listed in the table, a "−1" is returned.
Requires FlexDCA revision A.04.00 and above.