Jitter Definition Measurement Commands
Meas. mode:
Jitter
Package License:
L-RND
Waveform type:
NRZ
PAM4
Flex Apps:
FlexDCA
These commands linked from this topic configure jitter and amplitude measurements.
The Pattern commands allow you to specify the BERT pattern in Jitter mode. Using the :MEASure:PATTern:MODE command, you can specify that the pattern (NRZ or PAM4) be automatically detected, specified to be a known pattern, or a pattern loaded from a BERT pattern file (*.ptrn). These commands are similar to the pattern commands that are used to specify the pattern for a signal processing Decision Feedback, Linear Feed Forward, or TDECQ Reference equalizer operator.
Deprecated Commands
- :MEASure:JITTer:DEFine:LEVel:CUSTom (deprecated)
- :MEASure:JITTer:DEFine:LEVel:PERCent (deprecated)