Top/Base Configuration
Meas. mode:
Scope
Eye
TDR
Flex Apps:
FlexDCA
FlexRT
In Oscilloscope, Eye/Mask, and TDR/TDT Modes, a waveform's top and base definitions for measurements can be set proportional to the signal amplitude or set to user-defined values using the :MEASure:TBASe:METHod command. Custom values are specified, depending on waveform source, by the commands listed in the following table.
| Waveform Type | Commands |
|---|---|
| Channels | :CHANnel:UDEFined:BASe
:CHANnel:UDEFined:TOP |
| Differential Waveforms | :DIFF:UDEFined:BASe
:DIFF:UDEFined:TOP |
| Eye Memory | :EMEMory:UDEFined:BASe
:EMEMory:UDEFined:TOP |
| Waveform Memory | :WMEMory:UDEFined:BASe
:WMEMory:UDEFined:TOP |
| Function | :FUNCtion:UDEFined:BASe
:FUNCtion:UDEFined:TOP |