:WMEMory:UDEFined:BASe
Instrument:
N1000A
N109x
UXR Scope
Flex Apps:
FlexDCA
FlexRT
Meas. mode:
Scope
Eye
Jitter
TDR
Waveform type:
NRZ
PAM4
Command Syntax
:WMEMory{1:8}:UDEFined:BASe amplitude
<amplitude> is a double.
Where the {1:8} specifier identifies one of eight possible waveform memories. For example, :WMEMory4.
Query Syntax
:WMEMory{1:8}:UDEFined:BASe?
Description
For the indicated waveform memory, sets the custom base-level. The top and base levels are used to locate a waveform's lower, middle, and upper threshold levels during the following measurements: duty-cycle distortion, rise time and fall time. Specify the level in volts or Watts depending on the waveform type. Use :WMEMory{1:8}:UDEFined:TOP to set or query a custom top level.
Before this custom base level can be applied to measurements, use the :MEASure:TBASe:METHod command to select custom top-base definitions.
Example Command Sequence
:MEASure:TBASe:METHod UDEFined :WMEMory2:UDEFined:BASe -125E-3 :WMEMory2:UDEFined:TOP 125E-3