:MEASure:TBASe:METHod
Meas. mode:
Scope
Eye
TDR
Flex Apps:
FlexDCA
FlexRT
Command Syntax
:MEASure:TBASe:METHod {STANdard | UDEFined}
Query Syntax
:MEASure:TBASe:METHod?
Description
Selects the method used to define a waveform's top and base definitions. The command is equivalent to setting in the Top-Base Definition tab in the Configure Measurements dialog.
- STANdard
- Specifies that the levels be automatically determined. The top (100%) and base (0%) levels are relative or proportional to the signal amplitude. This is the default setting.
- UDEFined
- Allows you to enter absolute values for the top-base levels. When
UDEFinedis selected, use the commands shown in the following table to enter the top and base levels depending on the waveform type.
| Waveform Type | Commands |
|---|---|
| Channels | :CHANnel{N}:UDEFined:BASe
:CHANnel{N}:UDEFined:TOP |
| Eye Memory | :EMEMory{1:8}:UDEFined:BASe
:EMEMory{1:8}:UDEFined:TOP |
| Waveform Memory | :WMEMory{1:8}:UDEFined:BASe
:WMEMory{1:8}:UDEFined:TOP |
| Function | :FUNCtion{1:16}:UDEFined:BASe
:FUNCtion{1:16}:UDEFined:TOP |
| T-Domain and S-Parameter Traces in TDR/TDT Mode |
:TRACe{1:128}:UDEFined:BASe
:TRACe{1:128}:UDEFined:TOP |
| Instrument Mode | ||
|---|---|---|
| Oscilloscope | Eye | TDR/TDT |
| Average | Eye Amplitude | Average |
| Duty Cycle | Eye Height | Fall Time |
| Fall Time | Eye Width | Rise Time |
| Rise Time | One Level | Δ Time |
| Frequency | Zero Level | Time at Edge |
| Preshoot | Fall Time | Time at Amplitude |
| Oversoot | Rise Time | |
| Period | Crossing Time | |
| + Pulse Width | Δ Time | |
| — Pulse Width | Crossing % | |
| Δ Time | Duty Cycle Distortion | |
| Time at Edge | Signal to Noise Ratio | |
| Time at Amplitude | Jitter | |
| RMS | Extinction Ratio | |
| Amplitude at Upper | OMA at Crossing | |
| Amplitude at Middle | VECP | |
| Amplitude at Lower | Bit Rate | |
| OMA | ||
| Phase | ||
| Jitter | ||
Example Command Sequence
:MEASure:TBASe:METHod UDEFined :CHAN2B:UDEFined:BASe -125E-3 :CHAN2B:UDEFined:TOP 125E-3