:MTESt:SMODe
Command:
Deprecated
Deprecated command. For FlexDCA revision A.03.00 and above.
Command Syntax
:MTESt{N}:SMODe {XANDY | XONLy}
{N} identifies a specific mask and must be a value from 1 to 16. For example, :MTESt2: selects mask 2.
Query Syntax
:MTESt{N}:SMODe?
Description
Sets the mode for scaling the mask's X and Y axis ensuring that the mask will be properly loaded and adjusted on the screen.
XANDY- Specifies that both axis are scaled when the mask is loaded and aligned. The time value reference point (X) and vertical scaling points (Y) are adjusted. This parameter applies to all non-fixed voltage masks.
XONLy- Specifies that only the X-axes is scaled. This argument is designed for use on fixed voltage masks. Only the time value reference point (X) is adjusted. The vertical scaling points (Y) remain fixed.