:PTIMebase:RIPRogress?
Command:
Deprecated
Deprecated command for FlexDCA revision A.02.00 and above.
Query Syntax
:PTIMebase{1:4}:RIPRogress?
{1:4} identifies slot number which is associated with precision timebase.
Description
Queries if the external frequency reference is in the process of being detected.