:PTIMebase Subsystem
Instrument
N1000A-PTB
Flex Apps:
FlexDCA
Meas. mode:
Scope
Eye
Jitter
Module:
N1060A
The Precision Timebase subsystem commands control features available for the N1060A Precision Waveform Analyzer module. Be sure to include the module slot number (1 or 2) in the command string. For example, :PTIMebase{1 | 2}:STATe command SCPI subsystem node.
To control an N1000A-PTB internal precision timebase options, use commands found in the :TIMebase subsystem. Refer to :TIMebase:PTIMebase:STATe.
Commands in this subsystem requires an N1060A module.
As of FlexDCA revision A.08.30 and above, this subsystem no longer supports the 86107A precision timebase or 86108A/B precision waveform analyzer modules.