:SPRocess:AMPLify:GAIN

Instrument:
N1000A
N109x
Flex Apps:
FlexDCA
FlexRT
Meas. mode:
Scope
Eye
Jitter
TDR
Package License:
L-RND

Command Syntax

:SPRocessN:AMPLify:GAIN <gain>

<gain> is a double.

Where N identifies one of up to 64 possible operators {1:64} that can be defined as part of a math function. The operators are numbered in the order that they were originally added to the function.

Query Syntax

:SPRocessN:AMPLify:GAIN?

Description

Specifies the gain of an Amplify math operator.

Example Command Sequence

:FUNCtion2:FOPerator AMPLify
:SPRocess2:AMPLify:GAIN 1.5
:FUNCtion2:COLor TCOLor4
:FUNCtion2:DISPlay ON
*OPC?
…  //  Your code to synchronize execution timing.