:SPRocess:AVERage:ECOunt

Instrument:
N1000A
N109x
Flex Apps:
FlexDCA
FlexRT
Meas. mode:
Scope
Eye
TDR
Package License:
L-RND

Command Syntax

:SPRocessN:AVERage:ECOunt <count>

<count> is a int.

Where N identifies one of up to 64 possible operators {1:64} that can be defined as part of a math function. The operators are numbered in the order that they were originally added to the function.

Query Syntax

:SPRocessN:AVERage:ECOunt?

Description

Specifies the count of an Average math operator.

Example Command Sequence

:FUNCtion2:FOPerator AVERage
:SPRocess2:AVERage:ECOunt 64
:FUNCtion2:COLor TCOLor4
:FUNCtion2:DISPlay ON
*OPC?
…  //  Your code to synchronize execution timing.