:SPRocess:BUSer:LSTatus:REASon?
Instrument:
N1000A
N109x
Flex Apps:
FlexDCA
FlexRT
Meas. mode:
Scope
Eye
TDR
Package License:
L-RND
Query Syntax
SPRocess:BUSer:LSTatus:REASon?
Where N identifies one of up to 64 possible operators {1:64} that can be defined as part of a math function. The operators are numbered in the order that they were originally added to the function.
Description
Returns the reason for a failed load of a configuration file.
Use the :SPRocess{1:16}:BUSer:CFILe command to configure the function.
Requires FlexDCA revision A.05.00 and above.