:SPRocess:BUTTerworth:ORDer

Instrument:
N1000A
N109x
Flex Apps:
FlexDCA
FlexRT
Meas. mode:
Scope
Eye
Jitter
TDR
Package License:
L-RND

Command Syntax

:SPRocessN:BUTTerworth:ORDer <order>

<order> is a int.

Where N identifies one of up to 64 possible operators {1:64} that can be defined as part of a math function. The operators are numbered in the order that they were originally added to the function.

Query Syntax

:SPRocessN:BUTTerworth:ORDer?

Description

Specifies the order of a Butterworth filter operator. To configure the filter's Aliased Noise Processing, use the :SPRocess:BUTTerworth:PNOise command.

Example Command Sequence

:FUNCtion2:FOPerator BUTTerworth
:SPRocess2:BUTTerworth:BANDwidth 7.5E9
:SPRocess2:BUTTerworth:ORDer 2
:FUNCtion2:COLor TCOLor4
:FUNCtion2:DISPlay ON
*OPC?
…  //  Your code to synchronize execution timing.