:SPRocess:CONVolve:FRELoad

Instrument:
N1000A
N109x
Flex Apps:
FlexDCA
FlexRT
Meas. mode:
Scope
Eye
Jitter
Package License:
L-RND

Command Syntax

:SPRocessN:CONVolve:FRELoad

Where N identifies one of up to 64 possible operators {1:64} that can be defined as part of a math function. The operators are numbered in the order that they were originally added to the function.

Description

Reloads an S-parameter file for an Apply s2p operator. The file must have been previously loaded using the :SPRocess:CONVolve:FNAMe command.

Example Command Sequence

:FUNCtion2:FOPerator CONVolve
:SPRocess2:CONVolve:FNAMe "C:\Users<user_name>\Documents\Keysight\FlexDCA\S-Parameter Data\DUT_4.s2p"
:SPRocess2:CONVolve:FMODel ON  // Flips  S-parameters ports
:FUNCtion2:COLor TCOLor4
:FUNCtion2:DISPlay ON
……
:SPRocess2:CONVolve:FRELoad