:SPRocess:DELay:TIMe

Instrument:
N1000A
N109x
Flex Apps:
FlexDCA
FlexRT
Meas. mode:
Scope
Eye
TDR
Package License:
L-RND

Command Syntax

:SPRocessN:DELay:TIMe  <delay_time>

<delay_time> is a double.

Where N identifies one of up to 64 possible operators {1:64} that can be defined as part of a math function. The operators are numbered in the order that they were originally added to the function.

Query Syntax

:SPRocessN:DELay:TIMe?

Description

Sets the time delay for a Delay operator.

Requires FlexDCA revision A.01.60 and above.

Example Command Sequence

:FUNCtion2:FOPerator DELay
:SPRocess2:DELay:TIMe 10.6E-12
:FUNCtion2:COLor TCOLor4
:FUNCtion2:DISPlay ON
*OPC?
…  //  Your code to synchronize execution timing.