:SPRocess:GAUSsian:BANDwidth

Instrument:
N1000A
N109x
Flex Apps:
FlexDCA
FlexRT
Meas. mode:
Scope
Eye
Jitter
TDR
Package License:
L-RND

Command Syntax

:SPRocessN:GAUSsian:BANDwidth <cutoff_frequency>

<cutoff_frequency> is a double.

Where N identifies one of up to 64 possible operators {1:64} that can be defined as part of a math function. The operators are numbered in the order that they were originally added to the function.

Query Syntax

:SPRocessN:GAUSsian:BANDwidth?

Description

Specifies the cutoff frrequency in Hertz of a Gaussian filter operator. To configure the filter's Aliased Noise Processing, use the :SPRocess:GAUSsian:PNOise command.

Example Command Sequence

:FUNCtion2:FOPerator GAUSsian
:SPRocess2:GAUSsian:BANDwidth 7.5E6
:SPRocess2:GAUSsian:RISetime 52.4E-12
:FUNCtion2:COLor TCOLor4
:FUNCtion2:DISPlay ON
*OPC?
…  //  Your code to synchronize execution timing.