:TDR:SPMemory:SOURce
Command:
Deprecated
Deprecated command. For FlexDCA revision A.05.70 and above, use the :TDR:SPMemory:LOAD:SOURce command instead.
Command Syntax
:TDR:SPMemoryN:SOURce {DUT{1:16} | SPMemoryN}
Where N identifies one of four possible S-parameter memories. For example, :SPMemory3.
Query Syntax
:TDR:SPMemoryN:SOURce?
Description
Selects to load S-parameters into S-parameter memory from a TDR/TDT mode DUT-based setup (TDR mode only) or another S-parameter memory (Eye/Mask, Oscilloscope, or TDR/TDT modes). To actually load use S-parameters into memory, use the :TDR:SPMemory:LOAD command.
The query form of the command returns the current selected source.
Requires FlexDCA revision A.05.00 and above.
Example Command Sequence
// Loads S-parameters from DUT2 into memory 3. :TDR:SPMemory3:SOURce DUT2 :TDR:SPMemory3:LOAD // Loads S-parameters from memory 2 into memory 4. :TDR:SPMemory4:SOURce SPMemory2 :TDR:SPMemory4:LOAD