:TDR:SPMemory:LOAD:SOURce
Instrument:
N1000A
Flex Apps:
FlexDCA
Meas. mode:
Scope
Eye
TDR
Waveform type:
S-Parameter
Package License:
L-SNT
L-MFG
Command Syntax
:TDR:SPMemory{1:8}:LOAD:SOURce {DUT{1:16} | SPMemory{1:8}}
Where the {1:8} specifier identifies one of eight S-parameter memories.
Query Syntax
:TDR:SPMemory{1:8}:LOAD:SOURce?
Description
Selects to load S-parameters into S-parameter memory from a TDR/TDT mode DUT-based setup (TDR mode only) or another S-parameter memory (Eye/Mask, Oscilloscope, or TDR/TDT modes). To actually load use S-parameters into memory, use the :TDR:SPMemory:LOAD command.
The query form of the command returns the current selected source.
Requires FlexDCA revision A.05.70 and above.
Example Command
:TDR:SPMemory2:LOAD:SOURce SPMemory4