:TIMebase:PDCompensate
Instrument
N1000A
N109x
Flex Apps:
FlexDCA
Meas. mode:
Scope
Eye
Jitter
Command Syntax
:TIMebase:PDCompensate {ON | OFF}
Query Syntax
:TIMebase:PDCompensate?
Description
Turns Clock Pattern Distortion Compensation on or off. Clock Pattern Distortion Compensation compensates for coupling between the pattern and the recovered clock. FlexDCA automatically turns this setting on under the following situations:
- Keysight CDR hardware
- DCA-M or N1000A DCA-X timebase/sampling hardware used.
- Pattern locked with “Acquire Entire Pattern” selected.
It is recommended that you not change this setting unless performing a cross correlation.
Requires active support subscription for MFG or RND package license with F-PCOM feature (date 2022.0615).
Requires FlexDCA revision A.07.00 and above.