:WAVeform:PATTern:COMPlete?
Instrument:
N1000A
DCA-M
Meas. mode:
Scope
Eye
Flex Apps:
FlexDCA
FlexRT
Query Syntax
:WAVeform:PATTern:COMPlete?
Description
For pattern waveforms, queries the state of the trigger pattern lock. Zero (0) is returned if a pattern trigger is not established or if FlexDCA is not in Eye/Mask mode. Otherwise, returns one (1).
In Eye/Mask Mode (:SYSTem:MODE), requires pattern lock turned on (:TRIGger:PLOCk).
In Oscilloscope Mode (:SYSTem:MODE), requires pattern lock turned on (:TRIGger:PLOCk) and acquire entire pattern selected (:ACQuire:EPATtern). The waveform must be single valued. Single-valued waveforms represent a signal in which every horizontal acquisition point has associated with it one and only one amplitude value. In contrast, an eye diagram is displayed by measuring and displaying multiple amplitude values for each horizontal acquisition point.