Sin(x)/x

Instrument:
N1000A
N109x
Flex Apps:
FlexDCA
FlexRT
Meas. mode:
Scope
Eye
Jitter
TDR
Package License:
L-RND

The Sin(x)/x, or sinc(x), operator can be used to filter an input waveform. The default filter cutoff frequency is 7.5 GHz. Since some real-time oscilloscopes use a sinc(x) brick wall filter, you can use this filter to observe how the signal would appear on such an oscilloscope. Due to an increase in ringing, this filter tends to increase an eye diagram's height.

The operator's Display Setup configures the manner in which the resulting waveform is displayed including both vertical and horizontal scaling. For more information, refer to Common Display Settings.

The Preserve Noise setting compensates for the filter function's side effect of reducing a signals noise for adjacent measurement points. Selecting Preserve Noise causes the operator to quantify the noise on each point on the operator's input waveform and restore this noise on the corresponding data point on the output waveform. Because this increases the fidelity of the waveform, it is recommended that Preserve Noise be used. An example of an advantage of using this feature is during Mask testing, as without preserving the noise the mask hits counts may be too low (optimistic).

The Sin(x) / x operator requires a single-valued waveform, as opposed to an eye diagram. Be sure that your trigger setup results in a single-valued waveform at the input to this operator. This can be acheived using an external pattern trigger or by using pattern lock. If you are using an external pattern trigger, you may ignore this note.

Jitter measurements can be made on the Sin(x) / x operator's output waveform.