Available Time Domain Parameters
This informational dialog shows the time domain parameters (TDR responses) that are currently available for your specific DUT setup diagram (shown in the TDR Setup dialog). These available time domain parameters can be selected for display in the TDR Setup dialog and selected for calibration in the TDR Calibration dialog.
Responses that are currently unavailable for display can still be selected for calibration in the TDR Calibration Setup dialog.
Time domain parameters cannot be saved to a file.
For differential setups, the dialog shows both the available single-ended and differential time domain parameters that can be displayed and calibrated. For single-ended setups, the dialog only includes the available single-ended time domain parameters.
The dialog identifies all possible time domain parameters, which are determined by the number of ports on the DUT. Time domain parameters become available (highlighted) by activating TDR steps in the DUT setup diagram. Only those parameters that are highlighted are available for display. Parameters that are dim are not available. For example, in the above pictures, the T11 and TDD11 responses are available, but the T12 and TDD12 responses are not. To enable more responses, you must turn on the associated TDR steps in the DUT setup diagram.
The following examples show all of the time domain parameters that could be available for selected DUTs. If you are unfamiliar with time domain parameter names, you may find this section helpful.
Example of Time Domain Parameters on Single Ended 4-Port DUT
There are 16 possible time domain parameter responses for this DUT. When using an N1055A TDR module all 16 responses could be simultaneously displayed.
| DUT Setup Diagram | Time Domain Parameter | Response Description |
|---|---|---|
Port 1 Step: On![]() |
T11 | Return loss |
| T21 | Insertion loss | |
| T31 | Near-end cross talk | |
| T41 | Far-end cross talk | |
Port 2 Step: On![]() |
T12 | Insertion loss |
| T22 | Return loss | |
| T32 | Far-end cross talk | |
| T42 | Near-end cross talk | |
Port 3 Step: On![]() |
T13 | Near-end cross talk |
| T23 | Far-end cross talk | |
| T33 | Return loss | |
| T43 | Insertion loss | |
Port 4 Step: On![]() |
T14 | Far-end cross talk |
| T24 | Near-end cross talk | |
| T34 | Insertion loss | |
| T44 | Return loss |
Example of Time Domain Parameters on Differential 2-Port DUT
There are 16 possible differential and common-mode time domain parameter responses for this DUT. Because this is a differential DUT, 16 single-ended time domain parameter responses are also available. Therefore, a total of 32 possible time domain parameters are available for this DUT. When using an N1055A TDR module, all 32 responses could be simultaneously displayed.
| DUT Setup Diagram | Time Domain Parameter | Response Description | Time Domain Parameter | Response Description |
|---|---|---|---|---|
Port 1 Step: On![]() |
Differential Stimulus | Commom-Mode Stimulus | ||
| TDD11 | Diff. return loss | TDC11 | Diff. return loss | |
| TDD21 | Diff. insertion loss | TDC21 | Diff. insertion loss | |
| TCD11 | Comm. return loss | TCC11 | Comm. return loss | |
| TCD21 | Comm. insertion loss | TCC21 | Comm. insertion loss | |
Port 2 Step: On![]() |
Differential Stimulus | Commom-Mode Stimulus | ||
| TDD12 | Diff. return loss | TDC12 | Diff. return loss | |
| TDD22 | Diff. insertion loss | TDC22 | Diff. insertion loss | |
| TCD12 | Comm. return loss | TCC12 | Comm. return loss | |
| TCD22 | Comm. insertion loss | TCC22 | Comm. insertion loss | |
Example of Time Domain Parameters on Differential 4-Port DUT
For this DUT, a total of 128 time domain parameter responses are possible including 64 single-ended and 64 differential. There is a maximum limit of 64 responses can be acquired at a single time. So, when two N1055A modules are used, all eight cables are connected to the DUT but only two TDR incident steps can be activated.
| DUT Setup Diagram | Time Domain Parameter | Response Description | Time Domain Parameter | Response Description |
|---|---|---|---|---|
Port 1 Step: On![]() |
Differential Stimulus | Common-Mode Stimulus | ||
| TDD11 | Diff. return loss | TDC11 | Diff. return loss | |
| TDD21 | Diff. insertion loss | TDC21 | Diff. insertion loss | |
| TDD31 | Diff. near-end cross talk | TDC31 | Diff. near-end cross talk | |
| TDD41 | Diff. far-end cross talk | TDC41 | Diff. far-end cross talk | |
| TCD11 | Comm. Return loss | TCC11 | Comm. Return loss | |
| TCD21 | Comm. insertion loss | TCC21 | Comm. insertion loss | |
| TCD31 | Comm. near-end cross talk | TCC31 | Comm. near-end cross talk | |
| TCD41 | Comm. far-end cross talk | TCC41 | Comm. far-end cross talk | |
Port 2 Step: On![]() |
Differential Stimulus | Common-Mode Stimulus | ||
| TDD12 | Diff. insertion loss | TDC12 | Diff. insertion loss | |
| TDD22 | Diff. return loss | TDC22 | Diff. return loss | |
| TDD32 | Diff. far-end cross talk | TDC32 | Diff. far-end cross talk | |
| TDD42 | Diff. near-end cross talk | TDC42 | Diff. near-end cross talk | |
| TCD12 | Comm. insertion loss | TCC12 | Comm. insertion loss | |
| TCD22 | Comm. return loss | TCC22 | Comm. return loss | |
| TCD32 | Comm. far-end cross talk | TCC32 | Comm. far-end cross talk | |
| TCD42 | Comm. near-end cross talk | TCC42 | Comm. near-end cross talk | |
Port 3 Step: On![]() |
Differential Stimulus | Common-Mode Stimulus | ||
| TDD13 | Diff. near-end cross talk | TDC13 | Diff. near-end cross talk | |
| TDD23 | Diff. far-end cross talk | TDC23 | Diff. far-end cross talk | |
| TDD33 | Diff. return loss | TDC33 | Diff. return loss | |
| TDD43 | Diff. insertion loss | TDC43 | Diff. insertion loss | |
| TCD13 | Comm. near-end cross talk | TCC13 | Comm. near-end cross talk | |
| TCD23 | Comm. far-end cross talk | TCC23 | Comm. far-end cross talk | |
| TCD33 | Comm. return loss | TCC33 | Comm. return loss | |
| TCD43 | Comm. insertion loss | TCC43 | Comm. insertion loss | |
Port 4 Step: On![]() |
Differential Stimulus | Common-Mode Stimulus | ||
| TDD14 | Diff. far-end cross talk | TDC14 | Diff. far-end cross talk | |
| TDD24 | Diff. near-end cross talk | TDC24 | Diff. near-end cross talk | |
| TDD34 | Diff. insertion loss | TDC34 | Diff. insertion loss | |
| TDD44 | Diff. return loss | TDC44 | Diff. return loss | |
| TCD14 | Comm. far-end cross talk | TCC14 | Comm. far-end cross talk | |
| TCD24 | Comm. near-end cross talk | TCC24 | Comm. near-end cross talk | |
| TCD34 | Comm. insertion loss | TCC34 | Comm. insertion loss | |
| TCD44 | Comm. return loss | TCC44 | Comm. return loss | |