:EUSage:END
Flex Apps:
FlexOTO
FlexOTO Instance:
Hardware Diagram
Command Syntax
:EUSage:END <date-time>
Where <date-time> is a string in the format mm/dd/yyyy hh:mm:ss.
Query Syntax
:EUSage:END?
Description
Sets the end time of the diagram's view port. The recorded data is not clipped. The format of the time argument is in the same format as is shown on the diagram for End:
mm/dd/yyyy hh:mm:ss
Example
hwdiagram.write(':EUSage:END 04/23/2023 08:17:05')