:EUSage Subsystem

Flex Apps:
FlexOTO
FlexOTO Instance:
Hardware Diagram

Use the :EUSage subsystem to modify the x-axis of the Job Timing Diagram and to return time durations for tasks shown in diagram. The Job Timing Diagram shows data for all Stations and continues to record time until Stop FlexOTO Stations is clicked (Hardware Diagram's :STOP root command). Use a scroll-wheel mouse to reduce the diagram's x-axis viewport to be less that the data record. Note that if you have installed a generic instrument, the results for the instrument will be included in the diagram.

The diagram's start time can be set and queried using the :EUSage:STARt, :EUSage:STARt:MINimum, and :EUSage:STARt:MAXimum commands. The end time can be set and queried using the :EUSage:END, :EUSage:END:MINimum, and :EUSage:END:MAXimum commands.

Use the :EUSage:PERCent and :EUSage:PERCent:VENGines commands to return the percentage of time consumed by tasks shown in the diagram. The value returned is the percent of the diagram's viewport.

:EUSage commands must be sent to the Hardware Diagram's VISA address and not to a Station's address.

Tasks Shown in Job Timing Diagram
Task Display Based On
Engines Fixtures
Acquisition Queue ■
Acquisition Engines ■
Analysis Queue ■
Analysis Engines ■
DUT Fixture N ■
Generic Instrument ■

To query process times for a specific Fixture's Lane during testing using a Station's Job ID, use the Station's :JOBS:RESults:INFO:TIMes? query. This query must be sent to a running Station.