:EUSage:PERCent:VENGines?
Flex Apps:
FlexOTO
FlexOTO Instance:
Hardware Diagram
Query Syntax
:EUSage:PERCent:VENGines?
Query Response
The following is a typical respone:
ACQUISITION QUEUE,ANALYSIS QUEUE,POWER METER (US123456PM),ACQUISITION ENGINE 1,ANALYSIS ENGINE 1,ANALYSIS ENGINE 2,ANALYSIS ENGINE 4,ANALYSIS ENGINE 3"
Description
Queries a list of all valid work engine task bar names on the Job Timing Diagram. These names can be passed as an argument to the :EUSage:PERCent query. The above example response includes "POWER METER (US123456PM)", which is a measurement instrument that was installed with an instrument driver.