:EUSage:PERCent
Flex Apps:
FlexOTO
FlexOTO Instance:
Hardware Diagram
Command Syntax
:EUSage:PERCent "<work-engine>"
Query Syntax
:EUSage:PERCent?
Description
Queries the percentage of time consumed by a work engine task (displayed task bar). This is the percent of time span of the viewport. The command argument is the name of the task shown on the Job Timing Diagram. For example, "Acquisition Engine 1". The argument is not case sensitive. You can use the :EUSage:PERCent:VENGines? query to return a list of all valid task names Job Timing Diagram.